This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS1018的采样精度和速率的问题

Other Parts Discussed in Thread: ADS1118
     采购了一批ADS1018IDGSR,测试了几个,发现有些参数与手册不符。使用之前申请的ADS1018IDGST样片正常,并未出现问题。
     问题陈述如下:
     1、AD采样不对。测试了几个13年的ADS1018IDGSR,发现有2个不能测试2mV以下的电压(采用的配置为PGA 16倍放大,单次转换,速率设置为3300SPS,ADC模式)理论上精度是0.125mV,2mV以下应该是可以测试的,之前申请的12年的样片ADS1018IDGST都是可以的。
     2、AD速率不对。后来我配置为连续转换模式,速率配置为3300SPS看了下ADS1018IDGSR的SO脚输出的波形,发现部分AD的采样时间不对(因为在连续转换模式下,SO会输出一个8u是脉冲来表示转换完成,以两个脉冲间隔确定周期),申请的样片为0.3ms(约为3.3KHz)与手册相同,有些片子的采样间隔为2.2ms(约为475Hz,这是ADS1118的速率,但是芯片上的丝印为BTNQ,ADS1118的丝印为BBEI)。
     目前测试的几个ADS1018IDGSR,AD采样不对的,速率都不对;反之不一定。
   
x 出现错误。请重试或与管理员联系。