Other Parts Discussed in Thread: ADS54J64, ADS58J64EVM, ADS58J64
您好,我们现在使用ADS54J64EVM+TSW14J56EVM两块电路板进行采样波形。遇到了几个问题,真诚的希望得到回复。
1、我们现在通过HSDC中的HSDCPro Automation DLL。使用Automation DLL C Example中的Get_Capture_Data_32bits函数得到了波形得数据。请问我们想要恢复成我们所采样的信号,我们应该对数据怎么处理呢?(通过HSDCPro Automation DLL User Guide,我们已经了解到“This function is used to get the captured sample data in an unsigned 32 bit integer array. Use this function if the sample resolution is higher than 16 bits and less than or equal to 32 bits. The samples of each channels are arranged in an interleaved format, E.g. If there are 4 channels, then the data should in the format 1,2,3,4,1,2,3,4,…”,)
2、我们在HSDC中有Chanel8,8个通道。经过测试发现ADS的四个采集通道的数据映射到HSDC的8个通道。AIN,BIN ,CIN ,DIN。分别对应Chanel 1,2;Chanel 3,4;Chanel 5,6;Chanel 7,8;那么举个例子。AIN得信号,对应Chanel 1,2,那么Chanel 1,2得数据具体有什么区别呢?我们肉眼只能能观测到两个数据得幅值差别很大。


3、我们从ADS得配置软件中看到了数据得过程。上面问题2中得Chanel 1,2是分别对应下图的I信号和Q信号吗?

我们再ADS54J64EVM芯片“ADS54J64 Quad-Channel, 14-Bit, 1-GSPS, 2x Oversampling, Analog-to-Digital Converter” “sbas841”文档中,看到关于DDC Mode0 只有下面一点描述。

。请问关于采样数据的这个调制过程是QPSK吗,或者有更详细的说明?通过Get_Capture_Data_32bits得到的数据,有具体的解调方法吗?我们又该怎么样去恢复出采样的原始信号?
4、从下面图片可知,我们adc的采样频率是Fs = 1GSPS,根据奈奎斯特采样定理,我们是不是可以最大采样500MHz的信号。图片中最后我们得到JESD204B位置的Fs = 250MSPS,请问最大能恢复多少频率的被采样信号?