我只是个刚接触这方面的学生,问的问题可能有点简单,可别笑话我啊。我用805E做了一个AD,考虑到单独抽出这个采样模块,所以并没有前端的跟随器电路。使用FPGA提供时钟信号,在实际测试中,采样率在1M时可以很好的工作,但达到5M时,采样就开始不跟着时钟的节拍了,一个时钟周期内随机的会采几个值;而且在测量正弦波时,有很强的噪声,但在测量方波时就没有。我的电路是根据datasheet接的。请问这会是什么原因造成的呢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
估计是时钟的上升和下降时间不满足ADS805的要求。手册第12页,时钟是5V电平逻辑,占空比要严格的50%,上升时间和下降时间要控制在2ns以内。我估计你在跑5M时钟时,上升时间和下降时间可能不满足要求了,在FPGA和ADC之间加一个驱动用的buffer,应该会好一些。