Other Parts Discussed in Thread: ADS8688A
您好,我用的ADS8688A芯片设计的8通道数据采集电路,测试发现REFCAP和REFIO引脚的电压都是3.78V,我在论坛里也看到有人提出了类似的问题,请问这是怎么回事?如何解决?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,使用内部参考,上电后,测得这两个电压都是在3.78V左右是吗?
REFIO和REFCAP接的这几个电容应尽量靠近引脚端,我看电路中好像并没有,实际layout是不是尽量靠近引脚端的?
另外有一点注意,就是REFIO和REFCAP参考的是REFGND,虽然您这里最终都接在AGND上,但是看内部电路buffer参考的是REFGND,防止由于实际layout时和GND之间有微小的压差导致出现输出电压不准的情况。
,
建议将RST/PD 引脚拉低至少400ns以上然后拉高,使得ADC进入power down状态之后恢复到normal operation状态,所有的寄存器恢复到默认值,然后再去测量下REFIO和REFCAP的电压是否还有偏差?