Other Parts Discussed in Thread: ADS8568
TI您好,大家好,有一个项目要求:吞吐量为510kSPS,16位精度。8个查分输入和16个单端输入。我们工程师选用的是ADS8568。两片ADS8568好像可以满足要求。但是我们的采集的信号是快速变化的模拟信号,输入变化很快的。要不要加一个采样保持IC呢。不加会有什么影响。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS8568
TI您好,大家好,有一个项目要求:吞吐量为510kSPS,16位精度。8个查分输入和16个单端输入。我们工程师选用的是ADS8568。两片ADS8568好像可以满足要求。但是我们的采集的信号是快速变化的模拟信号,输入变化很快的。要不要加一个采样保持IC呢。不加会有什么影响。
手册12页图4是等效输入电路,可以发现这个电路没有任何驱动能力,需要外部运放来驱动。如果前端信号源驱动能力足够,则前端只考虑滤波即可;如果前端信号源驱动能力一般,则可以参考手册39页电路图,加外部运放来做驱动。
TI您好!很感谢您的解答。TI公司里面的AD转换IC有很多,但是我们一直不清楚,什么时候需要加采样保持,什么时候不加采样保持?会不会对采集速率有影响?谢谢你们!
在模拟信号频率足够高的时候,比如100K的正弦波,我用一个正负30MA的驱动能力的放大器跟踪一下。可不用采样保持器吗,而直接进行模数转换吗?
呵呵,可能我比较啰嗦。不好意思,TI大侠哥哥姐姐们!你们辛苦啦!