Other Parts Discussed in Thread: ADS1247
配置:
WriteReg_S(Reg_MUX0|0x40, 0x00, 0x08); // Negative input AIN0 Positive input AIN1
WriteReg_S(Reg_VBias|0x40, 0x00, 0x00); // Bias voltage not enabled (default)
WriteReg_S(Reg_MUX1|0x40, 0x00, 0x30); // Onboard reference selected Internal reference is always on
WriteReg_S(Reg_SYS0|0x40, 0x00, 0x59); // 2000SPS the gain of the PGA 32
WriteReg_S(Reg_IDAC0|0x40, 0x00, 0x06); // current source that can be used for sensor excitation 1000μA
当温度升到50摄氏度左右时,数据立马变为负值,当温度恢复为常温时测值又恢复正常。A0和A1输入端电压是正确的。仿真程序,发现从ADS1247返回的值确实是负值。