This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dac900用opa637做iv转换

Other Parts Discussed in Thread: DAC900, OPA637, OPA211, OPA627

opa637连接如图,2脚接dac900互补电流。da的full-scale电流是20mA,当da的data输入0x000时Vout约为-1V,但是输入0x3FF是Vout才0.5V左右。如果把da的两个电流输出直接接50欧电阻到地,一个是1V,一个是0V,正常输出,接上opa637就不正常了,请问哪里出问题了。

  • 在Iout输出端口后面应该先加50Ω电阻到地,将电流信号转化为电压,再接入差分放大器。

  • 您好,OPA637是需要在增益大于等于5的情况下才能稳定工作的,所以像您的这个电路建议您使用OPA627,当然如果您感觉627的带宽不够的话,可以使用OPA211,或者去TI官网选购其他带宽更大的放大器。希望能够帮助您!