如题,ADC08D1520QML的采样率为最高3GSPS。那如果我要采集的信号的频率是1GHZ的,采集效果会如何呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,ADC08D1520QML的采样率为最高3GSPS。那如果我要采集的信号的频率是1GHZ的,采集效果会如何呢?
ADC08D1520在中国使用需要许可证,如果已申请许可证,请联系当地的TI技术支持解决。如果在没有许可证的情况下使用该芯片,TI不提供认可技术支持。
你好!
1.许可证是什么东东?如何申请?
2.我现在正在做选型,我需要采集一个大概500MHz左右的信号,请帮忙提供一款可以使用的芯片吧。
谢谢!
1. 12bit 200M以上,14bit 100M以上,16 bit 40M以上的ADC都是美国对华出口管制的,像这颗ADC08D1520,虽然只有8位,但是网站上看到是需要许可证(license)的。就是说,如果想在中国用这颗ADC,需向美国商务部申请license,否则TI原厂和正规代理商不会卖给你。
2. 500M指信号范围在0~500M,还是指中频500M,带宽可能没那么大?带宽要是没过200M的话,考虑一下ADS54T01或者ADS54T02。
您好!
我要采集的信号是指中心频率在500MHz,带宽范围大概在40MHz。
关于ADS54T01我看其Analog Input BW (MHz) 到1200MHZ,够高得,这个该怎么理解呢?