Other Parts Discussed in Thread: ADS1115, ADS7866
您好,我要对一个系统进行采样,需要分辨率是0.001V,我算了下12bitAD参考电压为4.096V时,分辨率为0.001V,满足要求,但是实际上电源的噪声电平峰峰值为20mV,所以我想问下,在这种20mV噪声电平的情况下,我采集来的电压能是准确电压吗?能采集到低于20mV下的准确值吗??应该怎么考虑AD采样位数和分辨率精度的问题???望解答
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,您的意思是说您输入信号上有20mV的噪声,还是AD转换器供电电源上有20mV的噪声啊?如果说信号上有噪声的话,建议您前级接一个低通滤波器,然后在采集,如果是SAR型的ADC,并且输入信号时低频的,可以多次采样求取均值等方法进一步降低跳动,如果是低速信号,建议您使用SD型的ADC,例如ADS1115,这种ADC有良好的低通特性,非常适合采集低频信号。如果是电源上有噪声,这个得看您的带宽了,ADC都有电源抑制比这个参数,电源的噪声会在ADC上有所抑制,至于具体抑制能力得看具体的片子和你信号的频率了。至于位数,理论上12BIT能顾满足您的要求,但是由于INL,DNL,以及噪声影响,12BIT ADC往往达不到实际精度,您可以选择16bit的。
谢谢您的回复,那是不是可以这么理解,当电源上存在20mV峰峰值的噪声电平的时候,此时如果AD的电源抑制比为6dB,那么进入AD的电源噪声电平就变为10mV了,可以这么理解吗?电源抑制比是不是这么用的
您好,是这么理解,但是电源抑制比是随着频率变化而变化的,所以对于不同频率的电源噪声有着不同的抑制能力,所以您可以参考您芯片datasheet的相关表格。
谢谢您的回复,那您的意思是说我原本想采样是达到12bit分辨率,现在需要选用16bit分辨率,那我采集来的16位数字信号,是不是应该只取16位数据的高12位作为我的采样结果,而丢失低4位信号,还是应该怎么样?我的意思是想请教下我需要12bit分辨率,但是按您说的选用16bit精度AD采样,那是不是将采集来的16位数字量只取其高12位,而丢掉低4位??谢谢您的回复。
您好,如果你只是需要12位的分辨率的话,您可以仍然使用12bit的ADC,我之前看您的信号较小,推荐16位是希望能够达到更好的分辨率和精度。既然您只需12bit的分辨率你可以使用12bit的,例如ADS7866等。当然,ADC都会存在一些INL和DNL以及OFFSET的误差,所以您根据您实际的精度要求来选择就可以了。