This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8728使用问题

Other Parts Discussed in Thread: DAC8728

你好,我在使用DAC你好,我在使用DAC8728时,为什么一直不能得到正确的电压输出,根据手册输入的偏置电压数据,偏置电压输出也不是一个正确的电压值。输入数据与输出电压不能和手册上的计算公式相吻合,比如输入0x2000,输出电压就已经达到最大值了,而实际上16位的DAC应该可以输入到0xFFFF,是什么导致这样的现象发生呢。我的USB,RSTEL信号选择任何一种组合,都不能按公式计算输出一个正确的电压值。

有可能是时序不正确吗,但是我是按着手册上的时序来的啊。

  • 你好!你的问题时DAC8728无法实现正常的电路功能,请确认下面信息:

    1)电源电压如何配置?

    2)时序图如何(时钟、数据和控制信号的关系)?

    3)寄存器配置?

    根据这些信息可以进一步判断问题可能在那里,谢谢!

    Steven

  • 谢谢你的回复。

    我的电源电压为+15V,-15V,参考电压为5V,IO电源电压为3.3V;

    数据线是正确的,因为读写寄存器是正确的,片选信号和写信号按照数据手册和EVM板的要求,片选信号为CS OR (XWE AND XRD),即将片选信号与相与过的读写信号相或以后输出;

    寄存器保持缺省状态或根据手册进行设置,现象没有太大变化;

    几个难以解释的现象是:在向DAC写数据时,BUSY信号一直为高,该信号用10K电阻上拉处理,但是是有电压输出的,只不过输出的电压不正确;另外,更改偏置电压寄存器,偏置电压输出引脚不能正确响应寄存器值。