现在项目设计,需要用到8路输出的DAC,每一路都可以配置成10KHZ的脉冲波输出(0-2.5V),dac128s085是3V供电,2.5V参考电压,请问这个DAC可以用吗?如何计算DAC的输出带宽,从那些参数可以看出?如果能提供计算方法,那就更好了,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在项目设计,需要用到8路输出的DAC,每一路都可以配置成10KHZ的脉冲波输出(0-2.5V),dac128s085是3V供电,2.5V参考电压,请问这个DAC可以用吗?如何计算DAC的输出带宽,从那些参数可以看出?如果能提供计算方法,那就更好了,谢谢!
您好,
关于输出电压范围,3V供电,2.5V参考电压,那么在输出接近0时会出现线性损失,具体见下面截图;如果是3V供电,3V参考电压,那么除了在输出接近0V时有线性损失,在接近电源轨3V时也会出现线性损失,具体见下面截图,这是所有放大器都会有的现象,因此 DAC128S085的输出放大器也不会例外。

关于DAC的输出带宽,DAC的更新率( update rate )将真正决定您可以使用此DAC实现的最大带宽,DAC128S085的更新率 由其参数settling time决定(SCLK速率不算特别低的话),即 1/8.5us=117KHZ。
DAC的更新率具体可通过settling time或数字接口(interface update time )来决定,具体判断方法请观看我们一个关于这个主题的视频:training.ti.com/ti-precision-labs-dacs-settling-time-and-update-rate
很抱歉回复晚了,前几天休假了
我现在是产生10KHZ的脉冲波,也就是要产生50us脉宽的高电平(2.5V);50us的低电平(2.5V),这样适用吗
您这里是说50us的低电平是指约为0V的低电平吧,如上所述,最低低电平达不到0V,只能说是接近0V。如果是这样的话,那么是可以的,看下 DAC128S085的压摆率SR是否满足您的设计要求: