dac80508的参考电压是不是只能设置成1.25或者2.5V这种,如果设置成0.625或者更小可以吗?
第二个问题,DAC80508的更新速率只有0.2MSPS,如果我的8个通道要输出10KHZ的脉冲波,占空比50%,能满足速率要求吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
1、如您截图所示,DAC80508 外部参考电压有输入范围要求,最小只能到1.2V,不能设置成0.625或者更小。
2、如果使用最大 50MHz SCLK时钟速度,则每个DAC数字code更新将需要大概0.48us(0.02us*24bits)。如果每个DAC需要单独更新,则需要3.84us才能更新所有8个DAC数字code。每个通道写入后,每个通道的settling time 将开始,除非您使用LDAC触发器同时更新所有DAC。(如果所有8个信道都需要相同的数据,则可以使用广播DAC寄存器同时对所有信道进行写入。)DAC80508的 settling time 按5us计算,则同步更新8通通一个数据需要3.84us+5us=8.84us
10KHZ的脉冲波,需要的更新率是20KSPS,更新一个数据需要的时间是50us,因此DAC80508是可以的。
更多关于 Settling time and update rate,请查看下面视频: