Other Parts Discussed in Thread: ADS127L01
datasheet的8.5.8节的菊花链操作章节,在figure8-36进行了菊花链连接举例。如下图

菊花链模式下,必须将引脚SDO/DRDY配置成“output-only”模式,我打算还是采用硬件的方式捕获“转换数据准备好”的信号,那么请问在菊花链模式下,引脚PIN14_DRDY从哪个ADC中引出来?是从最后一个“ADS127L11(4)”引出DRDY吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,菊花链连接的话,SDO/DRDY是从最后一个ADC中引出来没错,但是这个多重复用引脚 SDO/DRDY就只能作为SDO输出引脚,不再有DRDY功能。也就是SDO_MODE这里只能配置为0.

对于 SDO/DRDY的是否为dual mode还是only output mode的时序,您可以看下面这个时序图:

我的意思是菊花链模式后,引脚SDO/DRDY没有DRDY功能了,那么怎么知道什么时候开始读取数据。
如果用DRDY引脚作为DRDY功能,(是DRDY引脚不是SDO/DRDY引脚),那么这个DRDY引脚怎么连接
是的,用PIN14 DRDY来监测data ready信号。
是从最后一个“ADS127L11(4)”引出DRDY吗?
是的,最后一个device 引出来,其他DRDY 悬空。ADS127L01的数据手册对于SPI daisy chain模式介绍的比较详细,可以参考下:https://www.ti.com/lit/ds/symlink/ads127l01.pdf