This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电平转换器的速率

Other Parts Discussed in Thread: SN74AVC8T245, SN74ALVC164245

类似于SN74AVC8T245的数据速率:Max Data Rates

170 Mbps (VCCA < 1.8 V or VCCB < 1.8 V)和

320 Mbps (VCCA ≥ 1.8 V and VCCB ≥ 1.8 V) 指的是每一位的转换速率,还是8位的总数据速率?另外有些转换器没有指出速率,如SN74ALVC164245等,怎么换算?是1/tPHL么?

  • 为什么我用Hyperlynx仿真FPGA到SN74AVC8T245间的信号完整性,选用1.8VLVCMOS电平,PCB板中模拟走线传输延时为0.3ns,单通道的信号速率取50M以下时信号完整性稍好点;减小了走线的传输延时,信号完整性稍好点情况下的信号速率也不超过80MHz,所以怀疑这个

    Max Data Rates

    170 Mbps (VCCA < 1.8 V or VCCB < 1.8 V)和

    320 Mbps (VCCA ≥ 1.8 V and VCCB ≥ 1.8 V)

    指的8位总的信号速率,单位的可能是320bps / 8bit = 40bps。

    请您再确认一下!