This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC选型及采样方案

Other Parts Discussed in Thread: ADC108S052, ADC108S022, ADC108S102, ADS8332

我现在要做一款工业数据采集仪,需要采集8路4-20ma或者1-5v的模拟信号,被测信号频率不高,但是要求精度较高,需要12位以上的采样精度。目前正在做方案进行器件选型,请问:有没有性价比高的方案推荐。

目前能想到的方案有2,一、选一款带内部buffer的8路adc,但是没有发现合适的adc;二、采用多路模拟开关+运放+单路adc的方案,此方案电路相对来说复杂。

请问,我现在的这两种方案哪种更可行,或者有没有其他更好的方案,有哪些器件可以推荐?

  • 可以考虑一下ADC108S022,ADC108S052或ADC108S102。这些芯片都集成MUX,是单端输入。

    也可以考虑一下ADS8332,这颗芯片量程0~2.5V,如果1~5V的量程可以降低一些,则这颗芯片应该也可以满足要求。另外这颗芯片的MUX输出到ADC输入预留出了一个外部运放的接口,这个功能不错。