This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问一下ADS1601的参考电压是内部给效果好,还是外接好?谢谢
内部参考温漂有50ppm,还算比较大。
建议高精度的用外部的,你可以参考Ti的REF50xx系列,温漂在3ppm。
最好选择与信号源温漂相差不大的外部REF芯片,这样两者若漂移量成线性或近似线性,则可降低误差
我现在选择内部参考电压,用万用表量VREFP管脚是3.4V,量VREFN管脚是2.6V, VREF是0.8V,通过FPGA的I/O把REFEN拉低,PD拉高,我不明白为什么参考电压不对,是什么问题?