用ADS1118配置对热电偶的数据采集,热电偶的输入配置采用官方提供的2路输入搭配方式,系统配置为每隔250毫秒采集芯片上的温度,每隔50MS轮替采样2个热电偶数据。每次切换信道都会连续采样10个数据然后进行平均(由于首次采样的数据是上一信道的数据并非当次配置的数据所以丢弃)。时钟顶端占空时间1.5US,时钟底部占空时间为1.5US。系统配置采样速率860、连续转换模式,采样得到的数据不正常。用逻辑分析仪观察在每次切换成获取芯片本身温度模式后在紧接着的下一个获取数据点(即使调整间隔时间约50MS也未能解决问题)读取到的数据还是之前的数据,只有在连续注入5次配置数据后才可以度到芯片内的温度数据。如果将系统设置为单通道的数据采样模数时系统可以正常采样数据。