Other Parts Discussed in Thread: ADS1118
我现在在用DSP宇ADS1118IDST进行温度测试,读取ADS118里面的温度值时,始终是3752,对比说明书,算出环境温度为90多度,请问是否哪有问题]
1 我的DSP与ADS1118之间,按照ADS1118说明书51图接线。当通过DSP将ADS1118配置为电压模式的时候,
能够按照要求获得AN1与AN0之间的电压,与实际值一样,没有问题
2 我想获得ADS1118温度传感器值,给ADS1118发送如下指令:0X0E9B 0X0000的时候,从SPI口读到的
数据是:0x0EA8, 0x0E9B.
这是我配置为连续转换,温度模式的数据,将0X0EA8对应说明书的Table4的表格,算出环境温度为80度,而实际环境温度只有30度左右,
请问我的哪个地方出来问题
3 ADS118的电路板与DSP主控板上都无明显的发热元件,并保持良好的通风
4 如果需要通过热耦电阻获得被测物体的温度,我理解的方法是是:将ADS1118配置为电压采集的模式,
读出热电偶的电压,根据厂家的表格,查出对应电压的温度T1;然后将ADS1118配置为温度模式,
读取环境温度的数值,查ADS1118的温度表,得到环境温度T2。最后计算出实际的被测温度T=T1+T2?