This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS1211中DRDY信号

Other Parts Discussed in Thread: ADS1211

请问一下,DRDY在上电之后,也就是初始化后,是保持高电平还是低电平?在传送指令结束后,是不是会自动跳为高电平?麻烦用过ADS1211的给说一说,并且在用的过程中要注意的问题给我讲一下,在这里先谢谢大家啦!

  • ADS1211在Calibrate或者convert的时候DRDY都为高电平,Calibrate或者convert后会pull low.

  • 寄存器Command Register (CMR)的byte3的第0bit Data Ready bit 可以映射DRDY输出pin的电平状态。

    DATASHEET第21页:DRDY is forced HIGH prior
    to the DOR update, unless a read is in progress。就是说DRDY在DOR寄存器更新前(转换结束前)以及DOR READ过程的时候保持高电平。DOR更新后(转换结束后)就会自动变为高电平,而应该不是你所说的这传送指令结束后。

  • one converison period (转换周期)指对于master 模式来说

    ADS1210/11
    generates 8
    serial clock cycles
    and receives
    Instruction Register
    data via SDIO

    然后是

    ADS1210/11
    generates n
    serial clock cycles
    and receives
    specified
    register data
    via SDIO,这个conversion period结束后,DRDY才自动拉高。

    区别于master模式serial clcok由ADS1210/11自己产生,对于slave模式来说,serial clock 由外部device产生。

    以上内容datasheet 26到32页有详细说明。