This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

对DAC0832 datasheet典型电路的质疑



网友 damoyeren  在21icBBS 模拟技术 论坛问以下问题:

http://bbs.21ic.com/icview-620106-1-1.html

DAC0832的典型接法几点正确性的怀疑:
1.Iout2直接接地。电路输出端子直接接地违背常理,那样会烧坏片子。
2.LM336就这样简单的接下可以产生2.5v参考,不现实。需要接电源和限流电阻,加入5V的电源,限流电阻应该选多大?
3.ILE引脚置高,不可以直接接+15V电源。要么通过MCU给高电平控制信号,要么接限流电阻。直接接15v电源会烧坏IO吧?
4.如果将Vout输出又送进AD的一个转换通道,那么会不会烧坏IO,运放输出电流怎么算?AD输入通道灌电流是20ma。