我们在使用ADS1271做的数据采集卡中(±10V量程),信号通过OPA1632(使用单端模式)做1/4衰减后接入ADS1271,ADS1271使用高精度模式,通过改变ADS1271的主时钟来改变采样频率。
将输入端接地测零点时,改变采样频率,会有100uV的偏移,但在测ADR425出的基准源时,先最大采样频率修正增益误差,使采集结果为5000mV(uV级一直在跳,跳动量不到200uV),但改变采样频率时,如果采样频率大于80KS/S,采集结果都是5000mV,但是采样频率在50K时,为5015mV,然后,采集结果随采样频率减小而增加,采样频率减小到1Ks/s时,采集结果为5038mV,但是用万用表测,我的基准源信号都是5000mV不变的。
怀疑是我的调理电路出了问题,将ADS1271与前段的OPA1632断开,将基准源信号直接接进去,采集结果上仍然有上述随采样频率减小采集结果增加的问题。请问这是不是ADS1271芯片本身的问题?