This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在使用DAC9881EVM板及MMBO板时遇到问题

Other Parts Discussed in Thread: DAC9881EVM, DAC9881

您好!

在使用DAC9881EVM板及MMBO板时遇到问题:

1.当EVM与MMBO不相连,将MMBO的J12短接,J13两个跳线短接,J2供电,测试J5的电压值:J5.1输出5V,J5.2输出0V;

当EVM与MMBO相连,将MMBO的J12短接,J13两个跳线短接,J2供电,测试EVM板J6的电压值:J6.1输出5V;J6.2输出1.7V,过了一段时间J6.2测试3.5V;
这两块均是刚拆封的新板子,所以觉得很奇怪,为什么MMBO与EVM相接或者断开,EVM板的J6.2,也就是MMBO的J5.2输出结果不一致呢?

2.另外我还有两块EVM板,现在给它们供电后,dac9881非常烫,说明烧了吗?

其中一块的现象也很奇怪,我将跳线设置成双极性输出,正常情况输出范围应该是-10V到10V,但是实际测试结果显示:串行数据是1FFFF (h)时,TP3输出-8.1V,串行数据是20000 (h),TP3输出7.1V,同时我也测试了其他的几个点0FFFF,输出-4.4V,2FFFF,输出3.7V。dac9881一直非常烫。这块板子可能会存在什么问题呢?

  • 您好,

    在DAC9881evm的user‘s guide第17页写明:EVM的模拟供电需要外接,不是由EVM的母板供给。且J13两个跳线不能短接,确保断开。

  • 您好!我又拿了一块新的dac9881EVM
    直接给其供电:J6.1供12V,J6.2供-12V,J6.3供5V,J6.9供3.3V,跳线设置:W9的1、2短接,W11的1、2短接,w1的1、2短接,W5的2、3短接、W2的1、2短接,W12和W3短接,W3的1、2短接,W10的1、2短接,W6的1、2短接,J4的1、2短接,J1的1、2和7、8短接,J3的5、6短接,测量电压结果:W1是4.9V,W11是11.9V,J3的5、6是3.2V,TP8是5V,输入串行数据20000(H),W2是0.192V,W3是0.178V,TP3是
    -8.9V,输入数据1FFFF(H),W2是1V,W3是0.99V,TP3输出是-5.6V,这块板子是新的,芯片目前不烫,但输出的值不对啊

  • 您好!我又拿了一块新的dac9881EVM
    直接给其供电:J6.1供12V,J6.2供-12V,J6.3供5V,J6.9供3.3V,跳线设置:W9的1、2短接,W11的1、2短接,w1的1、2短接,W5的2、3短接、W2的1、2短接,W12和W3短接,W3的1、2短接,W10的1、2短接,W6的1、2短接,J4的1、2短接,J1的1、2和7、8短接,J3的5、6短接,测量电压结果:W1是4.9V,W11是11.9V,J3的5、6是3.2V,TP8是5V,输入串行数据20000(H),W2是0.192V,W3是0.178V,TP3是
    -8.9V,输入数据1FFFF(H),W2是1V,W3是0.99V,TP3输出是-5.6V,这块板子是新的,芯片目前不烫,但输出的值不对啊

  • 奇怪的是,难道这板子还需要预热吗,大约通电半小时,就可以正确输出了,说明接法和程序都没有错。但是断电约10分钟后,再给它供电,就又没有输出了,输出一直是0,dac9881的输出一直是2.45V,这是怎么回事儿呢?

  • 您好,

    有一点我问详细一点,就是你外部供电时使用:J13的两个跳线帽断开了吗? 是使用MMB0上的J14接口来外部供电吗? 需要供电正负15(12V也可以)以及+5V和GND。

    你的跳线帽设置写的很多,是默认设置吗?