This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7565使用问题

手册中关于SYNC的描述是:SYNC低电平时使能输入移位寄存器,SYNC需要保持低电平到接收玩24个SCLK周期才能更新DA输出,如果没到24个SCLK周期就变为高电平,输入移位寄存器将复位。

我可不可以这样理解,SYNC等于高电平时,移位寄存器为复位状态,低电平时为可使用状态。但是我在实际使用过程中,SYNC一直保持高电平使用可以正确DA输出,但是SYNC一直保持电平不能正确DA输出,输出一直为0。请问是我哪里理解错误了?SYNC这个IO脚在常态应该置为低电平还是高电平?

  • SYNC在数据输入的时候要保持低电平,24位数据输入完成之后DAC自动转换并输出,然后SYNC需要一个高电平后到低电平的转换(下降沿)开始另外24位数据的输入

  • 谢谢回答,我还有一些需要请教。在不需要输入数据时应该保持sync为低电平还是高电平呢?为什么呢?

  • 最后一组数据输入完成后可将SYNC拉为高电平,表示数据输入完毕;当在需要DA转换的时候直接将SYNC拉低,然后是数据输入