This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ads1298 Vrefp是-0.1V还是0V



MichaelSheep 发表于论坛 数据转换器

你好,

如您所说,程序在评估板上测试通过,所以基本可以先排除程序问题。

根据描述,您应该使用的是正负2.5V供模拟AVDD AVSS? 上电后VREFP由于内部buffer默认为不工作,所以Vrefp=AVSS=-2.5V.

但在您第三步,写入03h寄存器DC的时候,开启了bandgap的buffer,应该是会有-0.1V的电压的,而不是你测的0V。

方便的话,先写入03h值DC,将参考buffer打开,先不读数,测一下Vrefp是-0.1V还是0V? 我们一步一步往下排错

...............................................................................................................................................................................................................

你好

1 我测了一下 Vrefp是-0.1V

2 能否商量个时间段,集中解决一下问题    有点急

3 或者安排一下北京的技术支持协助我解决一下问题