This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5686的PLL问题

Other Parts Discussed in Thread: DAC5688

使用内部PLL模式,4x,CLK2悬空,PLLVDD接3.3V。

当CLK1输入频率小于50MHz时,PLL才能锁定,此时CPOUT电压约为600mV,当提高CLK1输入频率之后,就失锁了,观察CPOUT电压,该过程中首先是逐渐升高,到55MHz左右时突然升高到1.8V,此后就不再升高,并且CPOUT电压不再稳定,即失锁。

问题:

1. 为何高频率输入PLL不能锁定?环路滤波值已经做过多个方向的调整,均没有改善的趋势,都是在30~40MHz之间才能锁定;

期望能在输入121MHz时能够锁定。

2. VCO的压控范围是多少?为何到1.8V就不能再升高了?

配置字如下:


void Dac5686Cfg( void )
{
Dac5686Write( 0x02, 0x01 );
Dac5686Write( 0xb9, 0x02 );
Dac5686Write( 0x46, 0x03 );
Dac5686Write( 0x51, 0x04 );

Dac5686Write( 0x84, 0x07 ); // mode[1:0] div[1:0] sel[1:0] counter fullbypass
Dac5686Write( 0x07, 0x08 ); // ssb interl sinc dith sync_phstr nco sif4 twos
Dac5686Write( 0x00, 0x09 ); // dual_clk DDS_gain[1:0] rspect qflag PLL_rng[1:0] rev_bbus

}