如题,
我按附件里的原理图做好的板子,ads1211和C8051的接口参考的是datasheet里的FIGURE30的4线接法,并且上电顺序也是先AVDD后DVDD,但4,5分钟后ad就会发热,而且越来越烫。请问这是什么原因?
期待回复。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,
我按附件里的原理图做好的板子,ads1211和C8051的接口参考的是datasheet里的FIGURE30的4线接法,并且上电顺序也是先AVDD后DVDD,但4,5分钟后ad就会发热,而且越来越烫。请问这是什么原因?
期待回复。谢谢!
让你用示波器测一测的原因是因为很多细节的东西万用表测不到,万用表只能测很低频的东西。示波器能看到更多,比如纹波噪声等,可以详细检查你的ADC电源以及各个输出有什么问题,排除掉这些问题更好的定位问题。
每一片AD芯片基本都这么写:
The ADS1210/11 requires the digital supply (DVDD) to be
no greater than the analog supply (AVDD) +0.3V. In the
majority of systems, this means that the analog supply must
come up first, followed by the digital supply. Failure to
observe this condition could cause permanent damage to the
ADS1210/11.
Page 35