采用STATIC PGA模式配置AFE5801芯片时,99【2:0】为细调增益配置单元,99地址单元分别写的是24'h990009和24'h99000f,分别对应着0.125dB和0.875dB。对比0.125dB和0.875dB的测量结果,发现0.875dB时采集的信号和0.125dB时的信号差不多大,甚至略小。细调没有起作用。但是增益值都是写进去了的。只有两种可能性:一是控制码写的不对,二是芯片本身细调功能有问题?想请教一下原因...万分感谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用STATIC PGA模式配置AFE5801芯片时,99【2:0】为细调增益配置单元,99地址单元分别写的是24'h990009和24'h99000f,分别对应着0.125dB和0.875dB。对比0.125dB和0.875dB的测量结果,发现0.875dB时采集的信号和0.125dB时的信号差不多大,甚至略小。细调没有起作用。但是增益值都是写进去了的。只有两种可能性:一是控制码写的不对,二是芯片本身细调功能有问题?想请教一下原因...万分感谢!!!