This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1178时钟

Other Parts Discussed in Thread: ADS1178

看了ADS1178的数据手册,输入时钟CLK范围是100kHz到27MHz之间,SCLK推荐为CLK的1、1/2等

问题:

1、转换速率是否只与MODE有关,与输入时钟无关?若设置MODE为0,此时是无论输入时钟CLK为多少,转换速率都为10.5ksps么?

2、CLKDIV:1 = 27MHz; 0 = 13.5MHz (high-speed) / 5.4MHz (low-power);设置CLKDIV是否与输入时钟无关,只是影响tconv?

3、参考ADS1178的开发板,CLK为27MHz,是推荐值么?若使用25MHz有什么影响?

  • 你好,首先要保证输入时钟范围在100K-27M才能正常工作,然后转换速率与MODE和CLK有关,参考12页Table 3. 27M是最大值,若使用25M采样速率下降一点

  •  谢谢您的回答,那参照数据手册CLKDIV的管脚说明:1 = 27MHz; 0 = 13.5MHz (high-speed) / 5.4MHz (low-power);

    设置CLKDIV是否与输入时钟无关,只有 27MHz/13.5MHz / 5.4MHz这三种值,只是影响tconv?

  • 你好,CLKDIV是时钟分频设置,设置CLKDIV和MODE均是为了控制采样频率,采样频率是与MODE,CLK,CLDDIV有一个函数关系,即采样频率与这三个的值均有关系, 27MHz/13.5MHz / 5.4MHz这三种值是输入时钟CLK为27M时的值