This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.用ADS1278采集脑电、眼电及其肌电信号,是否有推荐的参考设计?
2. ADS1278是差分输入,前面的高精度,高输入阻抗,高共模抑制比的低噪声差分运放是否有合适的推荐?
您好,
1、很抱歉,我们没有使用ADS1278采集脑电、眼电及其肌电信号的参考设计,但是有 ADS1278EVM-PDK 评估模块,见下面产品链接:
https://www.ti.com.cn/tool/cn/ADS1278EVM-PDK
以及EVM 用户指南:https://www.ti.com.cn/cn/lit/pdf/sbau197
关于电生理信号(ECG, EEG, EMG)的采集,TI 有以下ADC产品,您可以了解下:
[FAQ] Does TI provide an overview for their Bio-Potential ADC portfolio?
2、在 ADS1278EVM中前级运放使用的是 THS4521,您可以先看下THS4521。
1.感谢你的回复,如果用THS4521,这个芯片的CMRR能到多少? 因为脑电信号比较弱,这个器件的噪声会不会把脑电给淹没掉呢?
2. 用THS4521 这个跟脑电帽是怎么样的连接方式呢? 脑电信号一般有3根,正,负,REF?下面这样的连接方式 有问题吗?
1、如下截图是3.3V下的CMRR曲线:
5V下的CMRR曲线:
下面视频有介绍全差分放大器的噪声计算和噪声控制,您可以根据方法评估下:
https://edu.21ic.com/video/2624
2、
2、REF电极是测量脑电信号的参考点,应该连接到测量通道的反向输入端,因此我认为这样连接没问题。
另外一点,脑电采集一般都要加右腿驱动,这样的全差分运放的话,是否也需要加呢? 如果加的话,应该是单独加一路接到脑电帽上吗?
您这里说的应该是病人偏置电极,用于偏置病人以设置EEG信号的共模信号。我建议您看下ADS1299EEG-FE EEG用户指南第7部分,以更好的了解EEG的测量原理,然后参考ADS1299EEG EVM原理图设计ADS1278测量电路。