我的ADS1112只能在单端模式下采集到AN0输入端的电压数据,无论我怎么配置控制字,采集到的数据都为AN0通道数据,配置控制字确实改变了,用在线仿真看的,刚开始以为片子坏了就换了个片子,还是和原来一样,请问这是怎么回事?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是的,芯片上电的时候也是只能采集到AIN0和AIN3的数据正常。我接的是电桥式压力传感器,如果我把差分输入接到AIN0和AIN1上,AIN2和AIN3悬空,采到的数据是0x0B8A,虽然不是负值但数据也不对,我差分端电压用表量了为4.5MV。
当AIN0和AIN1,AIN2和AIN3同时接上两个电桥时,采集到的AIN0和AIN1的数据就不是0x0B8A了,就变成了0xBC0E了,是一个负值。AIN2和AIN3接的是我用四个电阻搭的电桥,差分输出电压为0.216V。只有接AIN0和AIN3时采集到的数据才正常。焊了三个片子都这样,我打算换芯片了,折腾了半个月了,不知道什么原因,会是静电击穿了吗?