请教内容如下:
我们使用了两片DAC5670产生I/Q信号,DAC采样频率800MHz,但发现两片无法同步(每一次开机的结果不一样),因此:
1 是否有其他的芯片推荐?
2 是否能通过鉴别两路DAC提供给FPGA同步时钟的相位差的方法来解决,即鉴别出两路同步时钟相位异常时,给DAC560重新上一次电。这种方法是否可? 需要提到的是,我无法给时钟复位,因为始终来自于其他设备。
3 是否有其他更好的方法?
非常感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你的意思是,有时候启动刚好相差一个数据么,即芯片1输出DATAA的时候对应芯片2输出DATAB,而你想要的是芯片1输出DATAA且芯片2也是输出DATAA的数据?
因为你的频率是用在800M,毕竟你板子应该做好了吧,你可以先试试DATAA和DATAB短了,输入一样的值,然后频率增加到1.6G,思路就是把这两路当做一路用,这样你试试有效果没有。我再关注下有没有其他办法。