This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
1)我看你Reset直接接VDD,是不想用复位的功能么?还是处于其他考虑?复位功能我个人经验是在调试里要经常可能需要使用。
2)是滤波作用。
3)你看到文章是哪一篇呢,可能需要和实际情况而定。不过我不是很清楚你为什么把AINCOM端连在49.9欧那里,是处于什么考虑呢?另外为什么把参考源输入搞成差分的平衡的滤波器呢,是经验么?
4)测量单端信号需要把AINCOM接长GND或者某个固定已知电平。另外为什么不用ADS1255呢?
你好,
(1)我是参考ADS1256的Datesheet里Page28上的电路连接的,所以把参考源输入搞成差分的平衡的滤波器,我也不太清楚这样可以不。
(2)Datesheet里面说的在测单端信号的时候不能把AINCOM接地(Page14),要接到某个固定已知电平,所以就把AINCOM接到49.9Ω那里了,是不是应该接到2.5V参考电压那里就可以了?
(3)我需要测8路的单端信号所以要选ADS1256。
(4)在调试成功后的应用电路里,可不可以把Reset直接接VDD呢?
我是第一次接触这个AD芯片,可以给一些测量单端信号的参考电路吗?主要是单端信号输入那里该怎样连接?谢谢。。。