RT,我的控制芯片是FPGA,只有通道1工作,其他3个通道的PWDN置低,模式为高分辨,SPI,输出数据格式为fixed,TDM;***,CLKDIV置高。输出的DRDY是连续的周期信号,周期为20us,低电平大概为50~100ns。参考电压较稳定。
请问下大家,前提没有单端转差分模块,不论输入短接还是输入稳定直流电压,后12位都在跳动,这是为啥呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
手册上有写出(37页)需要转成差分信号才能获得手册上的性能。另外ENOB=(SNR-1.76)/6.02得出ENOB利用ENOB可以估计无噪声分辨率,即可估计最后的跳动位数。另外跳码,噪声可以从各个环节引入,所以最好能参考我们的EVM布局以及选料。
差分模块我不清楚你需要的是怎样的模块,我认为THS4521在手册上的参考电路里画出,应该满足你的要求。如果不满足的话可以写出你需要的指标,我们在帮你看看。