This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS830/831

Other Parts Discussed in Thread: ADS830

To TI:

在使用贵公司的ADS830/831芯片时,采样效果不理想。

在此提出问题:

1 FPGA给AD提供的CLK在80M时是否需要通过5V上拉把CLK信号增强。

2AD输出数据是否要加上电阻,实现阻抗匹配。

3射随出来后,接到AD 17脚 IN时  电阻要选50欧姆阻抗匹配,那电容是怎么选择的呢?

4贵公司有没有类似的demo,提供参考呢?

  • 1 FPGA给AD提供的CLK在80M时是否需要通过5V上拉把CLK信号增强。2AD输出数据是否要加上电阻,实现阻抗匹配。

    建议留电阻位置,在调试的时候根据系统实际情况来调整电阻的大小、有无。

    3射随出来后,接到AD 17脚 IN时  电阻要选50欧姆阻抗匹配,那电容是怎么选择的呢?

    芯片资料第8页有设计的参考电路,截止频率计算如下:

    F=1/(2*pi*R*C)通过这个公式来计算出电容电阻值。

    建议采用参考电路上的值。

    4贵公司有没有类似的demo,提供参考呢?

    申请demo的网站:

    focus.ti.com/.../ads8317evm.html

    希望可以对你有帮助。

x 出现错误。请重试或与管理员联系。