Other Parts Discussed in Thread: ADS1256
哪位大神可以说一下,通过AD芯片的哪些参数可以推算出对AD芯片供电的电源的纹波和噪声的要求啊?多谢了。。。
例如 ADS1256
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS1256
哪位大神可以说一下,通过AD芯片的哪些参数可以推算出对AD芯片供电的电源的纹波和噪声的要求啊?多谢了。。。
例如 ADS1256
首先,根据真有效位算出,对应一个LSB的电压值。如ADS1256的真有效位可达21.3位。+/-2.5V输入。对应电压值为2.384uV。我们理论上要求电源噪声对ADC噪声的影响要小于1/2LSB(这里LSB还是取真有效位吧)也就是要小于1.192uV。
然后,ADC也是有PSRR的。对ADS1256来说PSRR的最小值为60dB(1000倍)。但高频PSRR未给出,相信会更低。因此如果用60dB来算的话,则不应超过1.192mV(RMS值)。
进一步,如果使用24位的LSB来算,并且考虑电源的噪声是白噪声,ADC的高频PSRR会下降的因素的话。那对电源噪声的要求会高很多。
一般对于高精度ADC来说,必需使用低噪声LDO才能达到良好的效果。
不知这一解释。能否解决你的问题。