This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我这个月买了20个DAC8581为何调试一会就烧坏了,发烫。调试的时候还能正常工作呢,但是很多时候一开电源就发现不能工作,IC发烫。
你指的发烫,温度有多高,比较下相对环境温度的温升。DAC8581功耗就200mW多点,应该不会太烫。
另外,你把坏了的片子管脚AVss和AVdd, DVdd和DGND间量下,看有没有短路,和好的芯片对比下电阻有没有发生变化。
我检查了一下:DVDD=3.3V,AVDD=4.9V,VREF=4.9V,AVSS=-5.2V。不知是否正常?按照SPEC 上,都在范围内啊。你们每个电源建议多大,谢谢。
DAC8581的温升可以大致的估计一下。118度/W. 8581的最大功耗300mW以内,温升大约就0.3*118=35度。再加上你的环境温度,大致就是芯片的表面温度。
输出正常,芯片发烫的话,根据热阻计算下芯片的温度是否正常。TJ= PD*( RθJA) + TA; TA指的是环境温度,Pd指的是芯片的功耗,RθJA为热阻。