Other Parts Discussed in Thread: ADS1256, ADS1282, ADS1248
各位专家:
我目前在使用ADS1256,实测结果显示误差很到,输入模拟电压值 = 2.5000V,AD实际采集值 = 2.5320V, 相差约32mV;在其它几点测量,误差也较大。
电路图在附件中。不知道是不是因为没有设置好自校准参数?请专家帮忙分析原因,谢谢。
程序代码如下:
延时子程序:
void delay_12clk(void)
{ unsigned char i;
for(i=0;i<24;i++) ;
}
写寄存器子程序:
static void write_register(unsigned char reg,unsigned char wdata)
{
SPI1_send(WREG|reg); //选择写入寄存器
SPI1_send(0x00); //写入1个寄存器
SPI1_send(wdata); //写入数据
}
读寄存器子程序:
static unsigned char read_register(unsigned char reg)
{
static unsigned char x;
while(ADRDYB); //DRDY信号低时才能读寄存器
SPI1_send(RREG|reg); //选择写入寄存器
SPI1_send(0x00); //写入1个寄存器
delay_10us(); //延时10us 20130413添加
delay_10us(); //延时10us 20130413添加
x = SPI1_TranByte(0xFF); //读出寄存器值
return (x);
}
读ADS1256测量值程序:
unsigned long read_data()
{
unsigned char rx_dat[4]; long x;
while(ADRDYB);
rx_dat[0] = SPI1_TranByte(0xFF);
rx_dat[1] = SPI1_TranByte(0xFF);
rx_dat[2] = SPI1_TranByte(0xFF);
x = (long)rx_dat[0]*65536+(long)rx_dat[1]*256 +(long)rx_dat[2];
return (x);
}
初始化ADS1256子程序:
void INIT_ADS1256(void)
{
CS_SPI1 = 0; //选通SPI0
delay_100us(); //延时100us
while( ADRDYB); //20130417添加
SPI1_send(RESET); //复位 20130313
write_register(STATUS,0x06); //输出高位数据在前
write_register(MUX, 0x18); //MUX寄存器为默认值
write_register(ADCON, 0x20); //ADCON寄存器为默认值
write_register(DRATE,0xa1); // 1000sps 采样率
write_register(IO,0x00);
write_register(OFC0,0x00);
write_register(OFC1,0x12);
write_register(OFC2,0x02);
SPI1_send(SELFCAL);
delay_2us();
delay_2us();
delay_2us();
delay_2us();
}
ADS1256测试子程序:
void ADS1256_test(unsigned char *ADS1256_data_point)
{
unsigned long v = 0;
unsigned char i = 0;
CS_SPI1 = 0;
SPI1_send(SELFCAL);
delay_2us();
delay_2us();
delay_2us();
delay_2us();
while(ADRDYB); //DRDY信号低时才能读寄存器
write_register(MUX,0x38); //选择#3 channel
SPI1_send(SELFCAL);
SPI1_send(SELFOCAL);
SPI1_send(SYNC); //启动转换
delay_12clk(); //延时12clk
SPI1_send(WAKEUP);
delay_12clk(); //延时12clk
SPI1_send(SELFOCAL);
SPI1_send(RDATA);
delay_12clk(); //延时12clk
v = read_data();
*ADS1256_data_point = ((v & 0x00FF0000) >> 16);
++ADS1256_data_point;
*ADS1256_data_point = ((v & 0x0000FF00) >> 8);
++ADS1256_data_point;
*ADS1256_data_point = ((v & 0x000000FF) );
}