This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1118采信电压信号的问题

Other Parts Discussed in Thread: ADS1118

使用ADS1118手册SBAS457D的page1的电路,对直流电压信号进行测量,准备使用AIN0~AIN1,如何调整输入相关的元件参数?

是否2只1M的电阻取消、2只500R的电阻短接?

如果电源电压VCC为3.3V,是否page21的FS取2.048V?

信号电压是否为测量值乘以2.048V/65536?

  • 是的,如果你信号内阻不是很大,是可以这样接的,但是如果你信号内阻很大,建议前级加缓冲器。

    注意FS为正负2.048,所以计算时为2.048/32768.

  • 拆掉了2只1M的电阻,2只500R的电阻换成了0R,直接接入了一只电压不足的干电池,电池电压实测1.228V。

    写入0x8503,FS=正负2.048V,得到的测量值为0x5980且随着时间还有非常慢的降低,而0x5980/32768*2.048V=1.432V;

    写入0x8703,FS=正负1.024V,得到的测量值为0x4000且不变,不知该如何计算?

    写入0x8303,FS=正负4.096V,但工作电压为3.3V,得到的测量值为0x6CBD,如何计算测量值?

    如果输入的电阻从0R恢复为510R(手边没有500R的),则以上测量的结果变化如下:

    写入0x8503,FS=正负2.048V,得到的测量值为0x5963;

    写入0x8703,FS=正负1.024V,得到的测量值为0x4000且不变;

    写入0x8303,FS=正负4.096V,但工作电压为3.3V,得到的测量值为0x6CB0。