Other Parts Discussed in Thread: LMP90100
1楼已经重新编辑过,看1楼即可,2、3、4楼是调试过程中的一些信息,忽略吧,暂时保留先
求高人给点思路,问题有可能出在什么地方或者还有什么方法可以查找问题点
LMP90100电路按照官网上开发板设计,测量芯片电源正常、参考电压正常,测量芯片输入通道模拟电压(0)与实际符合
LMP90100+LPC1115(ARM Cortex-M0),LMP90100的D6做DRDYB,接到LPC1115的GPIO上,只扫描通道0,通道0用的是VIN0和VIN1,已经短接
代码根据官网上下的软件包移植而来(官网上控制器用的是MSP430)
程序大致流程:中断后置位标志位,while(1)循环检测标志位,如标志位置位,则读ADC采集结果
读ADC采集结果,测试过controlledstream、直读寄存器和normalstream三种方式,每次除三个转换结果寄存器外,还会读其他寄存器验证,主要是验证ADC状态(active、standby、poweroff)、ADC数据是否可用、当前通道号、CRC,验证用的寄存器每次不会全用到
三种工作方式下,目前验证的结果:1、通过串口输出的频率验证,ODR基本正确;2、通过外围LED显示结果,GPIO寄存器设定正确;3、以上两点,初步推断SPI接口基本正常;4、LMP90100工作不正常,通道号和采样结果有较大几率异常
LPC1115中断代码
void PIOINT0_IRQHandler(void)
{
if(((LPC_GPIO0->MIS) & (1u<<1))==(1u<<1))
{
LMP_ADCDataReady[0]=1;// set flag
LPC_GPIO0->IC |=(1u<<1);
}
。。。
}//中断程序经过多种方式验证:示波器、设其他标志位等,验证结果OK
第一种直接读寄存器
prev_URA = LMP90100_URA_END;
while(1)
{
if (LMP_ADCDataReady[0])
{
LMP_ADCDataReady[0] = 0;//clear flag
for(i=0;i<5;i++)
{
TI_LMP90100_SPIWriteReg(TI_LMP90100_GPIO_DAT_REG, i, &prev_URA);//GPIO测试,外接LED灯,验证结果OK
readtestbuf[i]=TI_LMP90100_SPIReadReg(0x19+i,&prev_URA);//读ADC,包括状态、数据、CRC,验证结果fail,读到的数据(通道和结果)乱七八糟
}
...
}
第二种是通过controlledstreamread,验证结果同直读寄存器,读到的通道号和结果乱七八糟
prev_URA = LMP90100_URA_END;
while(1)
{
if (LMP_ADCDataReady[0])
{
LMP_ADCDataReady[0] = 0; // clear flag
TI_LMP90100_SPIControlledStreamReadADC(addr, read_buf, 5, &prev_URA); // read status, adc output & CRC into read_buf
ch_status = read_buf[0]; // Get Channel Status byte
ch_num = ch_status & LMP90100_CH_NUM_MASK; // Extract Channel Number
adc_data = ((uint32_t) read_buf[1] << 16)
| ((uint16_t) read_buf[2] << 8) | read_buf[3]; // form raw adc output data
crc_test = TI_LMP90100_SPICRCCheck(read_buf, 4); // test if CRC read from device matches computed
...
}
第三种:normalstream,连续采样50次,其中通道号正确和数值合理(高、中字节是0x00,低字节忽略)的只有32个
count=4;
addr = TI_LMP90100_SENDIAG_FLAGS_REG;
while(1)
{
if (LMP_ADCDataReady[0])
{
LMP_ADCDataReady[0] = 0; // clear flag
TI_LMP90100_SPINormalStreamReadADC(addr, read_buf, count, &prev_URA);
for(i=0;i<4;i++)
{
UART0_Send(read_buf[i]);
}
....
下面是normalstram方式下寄存器的设定值
#define TI_LMP90100_RESETCN_REG_VALUE (0xC3) /* Register and Conversion Reset */ #define TI_LMP90100_SPI_HANDSHAKECN_REG_VALUE (0x01) /* SPI SDO High Z Delayed */ #define TI_LMP90100_SPI_STREAMCN_REG_VALUE (0x00) /* SPI Normal Streaming mode */ #define TI_LMP90100_PWRCN_REG_VALUE (0x00) /* Active Mode */ #define TI_LMP90100_ADC_RESTART_REG_VALUE (0x00) /* Disable restart Conversion */ #define TI_LMP90100_GPIO_DIRCN_REG_VALUE (0x47) //D6 D0-D3 output/*(0x40) D6 output, D0-D5 inputs */ #define TI_LMP90100_GPIO_DAT_REG_VALUE (0x47) // D6 D0-D3 high/* (0x40)Set D6 high, others ignore */ #define TI_LMP90100_BGCALCN_REG_VALUE (0x00) /* Background Calibration OFF */ #define TI_LMP90100_SPI_DRDYBCN_REG_VALUE (0x83) /* Enable DRDYB on D6, bits 0 & 1 must be 1, others default */ #define TI_LMP90100_ADC_AUXCN_REG_VALUE (0x20) /* bypass external clock detection, internal clock, select 0uA RTD current */ #define TI_LMP90100_SPI_CRC_CN_REG_VALUE (0x00) /* disable CRC, Bit 3 must be 0, DRDYB is deasserted after ADC_DOUTL is read */ #define TI_LMP90100_SENDIAG_THLDH_REG_VALUE (0x00) /* Sensor Diagnostic Threshold High */ #define TI_LMP90100_SENDIAG_THLDL_REG_VALUE (0x00) /* Sensor Diagnostic Threshold Low */ #define TI_LMP90100_SCALCN_REG_VALUE (0x00) /* System Calibration Control Normal Mode */ #define TI_LMP90100_ADC_DONE_REG_VALUE (0xFF) /* ADC Data unAvailable */ #define TI_LMP90100_SENDIAG_FLAGS_REG_VALUE (0x00) /* Sensor Diagnostic Flags - status output */ #define TI_LMP90100_ADC_DOUT2_REG_VALUE (0x00) /* ADC Conversion Data 2 */ #define TI_LMP90100_ADC_DOUT1_REG_VALUE (0x00) /* ADC Conversion Data 1 */ #define TI_LMP90100_ADC_DOUT0_REG_VALUE (0x00) /* ADC Conversion Data 0 */ #define TI_LMP90100_SPI_CRC_DAT_REG_VALUE (0xFF) /* Reset CRC Data */ #define TI_LMP90100_CH_STS_REG_VALUE (0x00) /* Channel Status */ #define TI_LMP90100_CH_SCAN_REG_VALUE (0x00) /* Single Channel Continuous Scan: Channel 0*/ #define TI_LMP90100_CH0_INPUTCN_REG_VALUE (0x01) /* diable sensor diagnostics, default ref, vinp 0 vinn 1 */ #define TI_LMP90100_CH0_CONFIG_REG_VALUE (0x40) /* CH0 Configuratio: 26.83SPS, FGA off, buffer in signal path*/ #define TI_LMP90100_CH1_INPUTCN_REG_VALUE (0x13) /* disable sensor diagnostics, default ref, vinp 2 vinn 3 */ #define TI_LMP90100_CH1_CONFIG_REG_VALUE (0x40) /* CH1 config: 26.835SPS, FGA off, buffer in signal path */ #define TI_LMP90100_CH2_INPUTCN_REG_VALUE (0x25) /* disable sensor diagnostics, default ref, vinp 4 vinn 5 */ #define TI_LMP90100_CH2_CONFIG_REG_VALUE (0x70) /* 214.65SPS, FGA off, buffer in signal path */ #define TI_LMP90100_CH3_INPUTCN_REG_VALUE (0x37) /* disable sensor diagnostics, default ref, vinp 6 vinn 7 */ #define TI_LMP90100_CH3_CONFIG_REG_VALUE (0x70) /* 214.65SPS, FGA off, buffer in signal path */ #define TI_LMP90100_CH4_INPUTCN_REG_VALUE (0x01) /* disable sensor diagnostics, default ref, vinp 2 vinn 3 */ #define TI_LMP90100_CH4_CONFIG_REG_VALUE (0x70) /* 214.65SPS, FGA off, buffer in signal path */ #define TI_LMP90100_CH5_INPUTCN_REG_VALUE (0x13) /* disable sensor diagnostics, default ref, vinp 4 vinn 5 */ #define TI_LMP90100_CH5_CONFIG_REG_VALUE (0x70) /* 214.65SPS, FGA off, buffer in signal path */ #define TI_LMP90100_CH6_INPUTCN_REG_VALUE (0x25) /* disable sensor diagnostics, default ref, vinp 6 vinn 7 */ #define TI_LMP90100_CH6_CONFIG_REG_VALUE (0x70) /* 214.65SPS, FGA off, buffer in signal path */ #define TI_LMP90100_CH0_SCAL_OFFSET2_REG_VALUE (0x00) /* CH0 System Calibration Offset Coefficient [23:16] */ #define TI_LMP90100_CH0_SCAL_OFFSET1_REG_VALUE (0x00) /* CH0 System Calibration Offset Coefficient [15:8] */ #define TI_LMP90100_CH0_SCAL_OFFSET0_REG_VALUE (0x00) /* CH0 System Calibration Offset Coefficient [7:0] */ #define TI_LMP90100_CH0_SCAL_GAIN2_REG_VALUE (0x80) /* CH0 System Calibration Gain Coefficient [23:16] */ #define TI_LMP90100_CH0_SCAL_GAIN1_REG_VALUE (0x00) /* CH0 System Calibration Gain Coefficient [15:8] */ #define TI_LMP90100_CH0_SCAL_GAIN0_REG_VALUE (0x00) /* CH0 System Calibration Gain Coefficient [7:0] */ #define TI_LMP90100_CH0_SCAL_SCALING_REG_VALUE (0x00) /* CH0 System Calibration Scaling Coefficient */ #define TI_LMP90100_CH0_SCAL_BITS_SELECTOR_REG_VALUE (0x00) /* CH0 System Calibration Bits Selector */ #define TI_LMP90100_CH1_SCAL_OFFSET2_REG_VALUE (0x00) /* CH1 System Calibration Offset Coefficient [23:16] */ #define TI_LMP90100_CH1_SCAL_OFFSET1_REG_VALUE (0x00) /* CH1 System Calibration Offset Coefficient [15:8] */ #define TI_LMP90100_CH1_SCAL_OFFSET0_REG_VALUE (0x00) /* CH1 System Calibration Offset Coefficient [7:0] */ #define TI_LMP90100_CH1_SCAL_GAIN2_REG_VALUE (0x80) /* CH1 System Calibration Gain Coefficient [23:16] */ #define TI_LMP90100_CH1_SCAL_GAIN1_REG_VALUE (0x00) /* CH1 System Calibration Gain Coefficient [15:8] */ #define TI_LMP90100_CH1_SCAL_GAIN0_REG_VALUE (0x00) /* CH1 System Calibration Gain Coefficient [7:0] */ #define TI_LMP90100_CH1_SCAL_SCALING_REG_VALUE (0x00) /* CH1 System Calibration Scaling Coefficient */ #define TI_LMP90100_CH1_SCAL_BITS_SELECTOR_REG_VALUE (0x00) /* CH1 System Calibration Bits Selector */ #define TI_LMP90100_CH2_SCAL_OFFSET2_REG_VALUE (0x00) /* CH2 System Calibration Offset Coefficient [23:16] */ #define TI_LMP90100_CH2_SCAL_OFFSET1_REG_VALUE (0x00) /* CH2 System Calibration Offset Coefficient [15:8] */ #define TI_LMP90100_CH2_SCAL_OFFSET0_REG_VALUE (0x00) /* CH2 System Calibration Offset Coefficient [7:0] */ #define TI_LMP90100_CH2_SCAL_GAIN2_REG_VALUE (0x80) /* CH2 System Calibration Gain Coefficient [23:16] */ #define TI_LMP90100_CH2_SCAL_GAIN1_REG_VALUE (0x00) /* CH2 System Calibration Gain Coefficient [15:8] */ #define TI_LMP90100_CH2_SCAL_GAIN0_REG_VALUE (0x00) /* CH2 System Calibration Gain Coefficient [7:0] */ #define TI_LMP90100_CH2_SCAL_SCALING_REG_VALUE (0x00) /* CH2 System Calibration Scaling Coefficient */ #define TI_LMP90100_CH2_SCAL_BITS_SELECTOR_REG_VALUE (0x00) /* CH2 System Calibration Bits Selector */ #define TI_LMP90100_CH3_SCAL_OFFSET2_REG_VALUE (0x00) /* CH3 System Calibration Offset Coefficient [23:16] */ #define TI_LMP90100_CH3_SCAL_OFFSET1_REG_VALUE (0x00) /* CH3 System Calibration Offset Coefficient [15:8] */ #define TI_LMP90100_CH3_SCAL_OFFSET0_REG_VALUE (0x00) /* CH3 System Calibration Offset Coefficient [7:0] */ #define TI_LMP90100_CH3_SCAL_GAIN2_REG_VALUE (0x80) /* CH3 System Calibration Gain Coefficient [23:16] */ #define TI_LMP90100_CH3_SCAL_GAIN1_REG_VALUE (0x00) /* CH3 System Calibration Gain Coefficient [15:8] */ #define TI_LMP90100_CH3_SCAL_GAIN0_REG_VALUE (0x00) /* CH3 System Calibration Gain Coefficient [7:0] */ #define TI_LMP90100_CH3_SCAL_SCALING_REG_VALUE (0x00) /* CH3 System Calibration Scaling Coefficient */ #define TI_LMP90100_CH3_SCAL_BITS_SELECTOR_REG_VALUE (0x00) /* CH3 System Calibration Bits Selector */