你好
关于ADS8588S增加外部保护电路的问题,在文档《sbaa462-Circuit for protecting ADC with TVS diode and PTC fuse》,中有比较详细的介绍。但是文档中提到的低电容的TVS管TSC公司PGSMAJ10CA,此型号已经停产。然后我找了很多其他厂商品牌,如TI,ONSEMI,DIODES,littlefuse等,都没有找到低电容的双向TVS管。请问,你们有推荐的吗?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好
关于ADS8588S增加外部保护电路的问题,在文档《sbaa462-Circuit for protecting ADC with TVS diode and PTC fuse》,中有比较详细的介绍。但是文档中提到的低电容的TVS管TSC公司PGSMAJ10CA,此型号已经停产。然后我找了很多其他厂商品牌,如TI,ONSEMI,DIODES,littlefuse等,都没有找到低电容的双向TVS管。请问,你们有推荐的吗?
谢谢!
您好,这篇文档中也提到了几款其他TVS的测试和PGSMAJ10CA的测试结果比较:可以看出PGSMAJ10CA的电容变化最小,THD的性能也最好。SMA6J10A和SMCJ10CA的电容变化相对来说要高一些。这三款的话可以看下SMA6J10A,虽然电容变化没有PGSMAJ10CA,但从测试结果来看可以考虑它。
或者联系下TSC公司的技术客服,看是否有和PGSMAJ10CA 能相互替代的TVS。

你好。你提到使用SMA6J10A,这个不是单向的TVS管吗?但是现在ADC输入是可以到±10V的,那这个是不是意味着需要用两个SMA6J10A串联起来使用吗?
是的,表中的这个测试结果,是采用了两个单向的SMA6J10A 使用的。
不客气,那我先把这个帖子关闭了,后续有什么问题,可以继续在这里跟进也可以重新建个新帖。