This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI读写ADS1293无效

Other Parts Discussed in Thread: ADS1293

这是我SPI读写ADS1293的程序,可以写入,示波器也能看见CS、CLK、MOSI都有方波波形,但是总是不能返回数据,我用中断模式去读取数据,DRDYB也不会被拉低,就是说没有返回数据,请高手看下,哪里有错误,或者可能是哪里的错误?

void ADS_Write(unsigned char ADS_COM,unsigned char ADS_DAT)
{
ADS_CS = 0;        // SSN LOW
U0DBUF = ADS_COM; while (!(U0CSR&0x02)); U0CSR &= 0xFD;
U0DBUF = ADS_DAT; while (!(U0CSR&0x02)); U0CSR &= 0xFD;
unsigned char temp = U0DBUF;
ADS_CS = 1;        // SSN high
}

/********************************
  从SPI器件读出一个字节数据
********************************/
unsigned char ADS_read(unsigned char ADS_addr)
{
unsigned char ADS_DAT;
ADS_CS = 0;        // SSN LOW
U0DBUF = 0x80+ADS_addr;
while (!(U0CSR&0x02)); U0CSR &= 0xFD;
U0DBUF =0x00;
while (!(U0CSR&0x02)); U0CSR &= 0xFD;

ADS_DAT = U0DBUF;
ADS_CS=1;
return ADS_DAT;
}

//初始化
  ADS_Write(0x01,0x11);  //IN1连CH1- ,IN2连CH1+
  Delay(1000);
  ADS_Write(0x02,0x19);  //IN1连CH2- ,IN3连CH2+
  Delay(1000);
  ADS_Write(0x03,0x2E);
  Delay(1000);
  ADS_Write(0x0A,0x07);  // 共模检测IN1,IN2,IN3.
  Delay(1000);
  ADS_Write(0x0C,0x04);  //通道IN4 为右腿驱动
  Delay(1000);
  ADS_Write(0x0D,0x01);  //威尔逊参考输入IN1
  Delay(1000);
  ADS_Write(0x0E,0x02);  //威尔逊参考输入IN2
  Delay(1000);
  ADS_Write(0x0F,0x03);  //威尔逊参考输入IN3
  Delay(1000);
  ADS_Write(0x10,0x01);  //威尔逊选择
  Delay(1000);
  ADS_Write(0x12,0x04);   //使能时钟  注意:设置此位高后,才振荡器起振后或振荡器已关闭和外部时钟已经开始了。
  Delay(1000);
  ADS_Write(0x21,0x02);  //抽取率?????
  Delay(1000);
  ADS_Write(0x22,0x02);
  Delay(1000);
  ADS_Write(0x23,0x02);
  Delay(1000);
  ADS_Write(0x24,0x02);
  Delay(1000);
  ADS_Write(0x27,0x08);   //Data Ready Pin Source  Driven by channel 1 ECG
  Delay(1000);
  ADS_Write(0x2F,0x70);  // 配置通道的环回读模式
  Delay(1000);
  ADS_Write(0x01,0x01);


void main(void)
{
    uchar count = 0;
    uchar LDate,MDate,HDate;
    uint ALLDate;
    Init_T4_AND_LED();
    INT_ADS1293();
    //Set_Spi();
    while(1)
    {

      LDate=ADS_read(TI_ADS1293_DATA_CH1_ECG_L_REG); 
      MDate=ADS_read(TI_ADS1293_DATA_CH1_ECG_M_REG);  
      HDate=ADS_read(TI_ADS1293_DATA_CH1_ECG_H_REG);
      ALLDate=LDate+MDate*255+HDate*255*255;  
    };