Other Parts Discussed in Thread: ADS5240, ADS58C48
各位老师好,我选择了一个ADS5240 ,4-Channel, 12-Bit, 40MSPS Analog-to-Digital Converter with Serial LVDS Interface,但是它的接口是Serial LVDS Interface,是不是不能与ARM直接连呢?应该要怎么接呢?请老师指导下!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
倒是有LVDS转TTL的你可以选择http://www.ti.com.cn/lsds/ti_zh/interface/lvds-phy-less-than-800-mbps-products.page#p995=&p996=&p994=1;16&p976=&p404=
但我觉得用ARM不知道合适不合适,因为每个码流如果是40M,bit速率会达到40*12M,这个速率不小而且是4路。不知你的ARM大概用什么接口来与之相连,满足ADS5240输出的时序。
一般情况下4通道的很少有并行输出的。因为需要的IO口台多了。如果12bit的ADC,4通道,简单的说就需要12*4+1=49个输出。这样的芯片的封装就会很大。
你可以看看ADS58C48。他可以配置成CMOS并口输出的。虽然是11bit的ADC,但是内部是14bit的核心,性能很号的