大家好!这边正在使用ADS8363EVM+FPGA的方式测试AD性能,由于需要采用差分输入,并且要求两路同步采样,考虑之后打算使用Mode I,外部提供2.5Vref,只接到REFIO1上,采用A0和B0两路输入通道,测试短路噪声时(A0-和A0+、B0-和B0+短接),原本以为收到数据应该都为0的,可是发现收到的数据都为7FFF,在输入端加入10K、1Vpp、1Voffset时,收到的数据出现限幅现象,如下图所示:
当输入信号为10K、1Vpp、0.2Voffset时,收到的数据如下图所示:
当输入10K、1Vpp、0.5Voffset时,采集到的数据正常。
测试ADC上电管脚状态,发现A0+、A0-、B0+、B0-、CMA、CMB为1.5V的样子,REFIO1、REFIO2上都为2.5V,这边只在上电的时候发送啦一次SDI = 0x1000,用于配置通道0,工作模式应该是正确的吧?查看数据,有点像符号位丢失或高位丢失,原因还在查找中,希望有专家可以提供下帮助,谢谢!