我们公司向用贵公司的ths8200做一款1080P的VGA输出视频,要求输入是BT1120输入,VGA输出。这款ths8200能支持吗?那么低8bit数据是接在GY接口上,高8bit数据接在BCB接口上吗?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们公司向用贵公司的ths8200做一款1080P的VGA输出视频,要求输入是BT1120输入,VGA输出。这款ths8200能支持吗?那么低8bit数据是接在GY接口上,高8bit数据接在BCB接口上吗?谢谢!
Hi baoqiong,
Yes, the THS8200 does support BT.1120 1080p-30Hz. The setup will be similar to 1080p-60Hz, but the pixel rate and clock will be 74.25MPPS instead of 148.5MPPS.
In general, BT.1120 with embedded syncs is supported by setting the input format to 20bit YCbCr 4:2:2, enabling the 4:2:2 > 4:4:4 interpolation filter, and enabling embedded EAV/SAV sync operation. Other settings such as pixels per line, lines per frame/field, dtg_spec_x horizontal timing, and output sync amplitudes must be uniquely set depending on input format.

Hi baoqiong,
THS8200 should support 1080p VGA,please check attached file for the setup.