Other Parts Discussed in Thread: DAC7724, DAC7716
DAC7724芯片资料上介绍VCC电压为15V,我现有的电路板接15V比较困难,我想问下给VCC接12V可以不?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
从手册上看,TI不能保证VCC=12V时候的性能,没有针对这一电压供电进行测试。从测试数据中也可以看出。可能在输出的电压或者电流的大小上和15V供电时候不一样。
不知你的应用是什么场合,需要怎样的具体需求,看看是否能为你推荐一款其它的芯片。
我想要用输出0-10V模拟信号,设备上现在只能提供正负12V的电源电压。并行,串行I2C都可以!谢谢 !!
我认为DAC7716这方面能满足你的要求。但总线是SPI的,不是I2C。I2C的比较少。
另外一种方案是I2C的DAC加上一个运放进行放大也能达到0-10V输出。
28335有应该不止一个MCBSP,这个有时候比SPI更好用,可以配置成SPI的时序。