Other Parts Discussed in Thread: ADS1255, INA105, OPA188, OPA4188, OPA2188, INA128, TINA-TI
最近我想用ADS1255做一个测量电流值的设备,电流用取样电阻转成电压信号,但是不知道用什么样的放大器做前端来驱动ADS1255,请大家推荐一款,谢谢!电流值只有几十毫安,正负电流都会出现,系统带宽要求很低,1K左右就差不多,关键希望有高精度和低噪声。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
ADS1255内部有PGA,可编程增益的放大器,最大可以64倍。不知道你用多大的采样电阻来I/V转换呢?你算算这个PGA能满足你的应用吗?
如果不能满足,你是在高端采样能还是在低端采样?如果高端大概多大的共模电压,可以选择仪表放大器一类,如果低端采样,通用运放也可以选择。
你的采样电阻还挺大的,最大电压时正负10V么,50mA和200欧电阻乘法一下好像还挺大的?!能确认下么是这么大么。
如果有正负电压你可以考虑用INA105这种差分运放来抬升电平,也可以自己用精度较高的通用运放和精密电阻搭一个差分放大器。
OPA188不错,漂移极小,供电宽,噪声低。双运放和四运放版本是OPA2188,OPA4188。这款运放很流行。
http://www.ti.com/lsds/ti/amplifiers-linear/dual-supply-products.page?paramCriteria=no
这个网址可以查,INA128应该不错。需要注意的是得选个双电源的仪表放大器,你要提供正负电源,因为输入有负的电压。
另外TINA-TI仿真软件可以仿真一下,确认一下。