Other Parts Discussed in Thread: TMUX6121

工程师您好!我最近在使用DAC7718芯片进行数模信号转换并选择从不同的通道输出信号,我使用51单片机对DAC7718输入信号,DAC7718的连接参照EVM进行,如上图。目前的问题是信号无法识别,输出通道无信号输出或者没有通道选择特性,A组4个端口的均有输出。请问着是否是上电时序的问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
您现在问题是A组4个端口输出正常?B组输出通道无信号输出?
AVDD, AVSS, DVDD, IOVDD , REF-A , and REF-B 供电电压分别是多少?实际测量正常吗?
您是双极性应用吗?OFFSET-A 和OFFSET-B是怎样接的?
上电顺序不正确可能会造成一些问题,下面链接是我找到的用户上电不正确遇到的问题:
在您的应用中,上电顺序是怎样的?

工程师您好!我目前遇到的情况是,假如我选择了A组的out2端口输出,那么整个A组的输出端口out0-out3都有同样的输出信号。而且这并不稳定,有时候表现为无任何信号或者A组输出端口全部输出AVSS的电压。
我的AVDD为+12V,AVSS为-12V,IOVDD和DVDD、REF-A/REF-B全部使用5V的电压供电,我采用的确实是双极性应用,根据数据手册建议,OFFSET-A和OFFSET-B没有做任何连接。
我按照IOVDD和DVDD连一起上电,AVDD/AVSS,REF-A/B的顺序进行上电,但是结果并不对,单片机时序没有问题,数字信号幅值也没问题。而且芯片发热非常严重。我的上电时序是利用杜邦线一个接一个插入来实现的,我想问题可能出在这里。另外,由于只需要输入信号,SDO接口我没做任何连接。麻烦您看一下我的连线有没有问题。下面是我的单片机输出时序,也请您帮我看一下。
从上到下依次是LDAC、CS、SCLK、SDI

下图是单片机的SDI引脚输出电平

关于TMUX6121,您说的是下面链接中的问题吗?现在TMUX6121是否正常工作了?
https://e2echina.ti.com/support/switches-multiplexers/f/switches-multiplexers-forum/530328/tmux6121
对的,先解决DAC7718上电顺序的问题,您的这个思路是对的。