我在使用ADC122s021的时候发现,模拟输入驱动需要一个低阻抗的源,这样可以减小失真度,请问则个低阻抗源的抵抗范围是多少比较合适?现在我使用OPA2376来驱动这两路信号,OPA2376的开关输出电阻式150欧,请问是否可行?另外,怎么样尽量降低ADC122s021两路之间的串扰问题。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在使用ADC122s021的时候发现,模拟输入驱动需要一个低阻抗的源,这样可以减小失真度,请问则个低阻抗源的抵抗范围是多少比较合适?现在我使用OPA2376来驱动这两路信号,OPA2376的开关输出电阻式150欧,请问是否可行?另外,怎么样尽量降低ADC122s021两路之间的串扰问题。谢谢!
您好,ADC122S021是SAR型ADC,其内部有采样保持电路,所以需要对采保电路充放电,无疑这需要比较大驱动电流。由于运放具有高输入阻抗低输出阻抗的特性,所以采用放大器作为SAR型ADC的驱动是比较常用的方式。OPA2376是一款低功耗的轨至轨输入输出型运算放大器,其良好的直流参数以及低噪声特性可以很好的用作ADC buffer,所以采用OPA2376是没有问题的。
您可以把串扰理解成一个噪声源,只要串扰带来的影响不高于噪底,在大多数情况下,都不用考虑这个问题。测试串扰,可以把A通道输入短接,然后在B通道送入信号。这时候在A通道可以观察到B通道带来的串扰,一般情况下,这个串扰都不会超过噪底的,更何况ADC122S021具有86dB通道间串扰抑制。在布信号线时尽量保证各个通道信号线的等长、等间距,尽量平行走线并保持整体的对称性。划分数字、模拟电源、地并在多层板中使用完整的电源、地。如果已经观察到串扰现象,最好分析串扰的耦合路径,然后从信号、电源、地的处理以及增加一些滤波、屏蔽元件上入手。