This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1232的问题

Other Parts Discussed in Thread: ADS1232

您好!我最近在使用ADS1232做一个电子称时遇到下面的问题,请指点: 1,我使用的是数据手册上的P25中的figure 42.因为我用的MCU是5V供电的,所以图示中的3V电源也是5V,也就是电路中的电源就只有一个5V实现,但是我在使用中发现,MCU能够检测到数据准备好信号,只是程序读出的24位数据全是1。我把ADS1232的11,12脚短接了输了出还是全是1,我给ADS1232的11,12脚外接输入一个差分3毫伏的信号,输出还是全1。我想是不是这个芯片坏了。(我没有做电路板,只是用一个贴片转直插的板子,将ADS1232转成直插用万能板接成图示电路)。 2,我在数据手册上看到P18关于此转换器的LSB的定义感到不能理解:0.5VREF/(223 – 1).这里的分母为什么要减个1呢,我觉得不应该减1啊? 谢谢指点 2014.2.20
  • Hi Ping,

       能否提供一下读取数据时的波形?

       因为ADS1232的满刻度是7FFFFFh,所以一个lsb是0.5VREF/(2^23 – 1).

  • 谢谢您的回答,最近出差现在才来继续这个问题,今天发现无法读取数据了,也就是说表示数据准备好的DOUT端一直出不了低电平,发现本来调好的直流稳压电源5V加给1232后发现只有3V了,想想肯定坏了吧,就换了第四块1232,发现还是一样的问题(表示数据准备好的DOUT端一直出不了低电平),我现在的问题是:

    1.我在前面的焊接过程都是用普通铬铁焊接的,想咨询一下是不是静电将1232损坏了,这个芯片抗静电能力就这么差吗?。
    2.今天在换1232时候,我便采用防静电镊子拿捏芯片,用热风枪吹焊(近400度的温度)。结果接上去还是不行,如果不是静电损坏,这次是高温损坏了吗?我该怎么操作才行呢?谢谢您的建议。

  • 你好,请问解决了吗?我也出现这种问题

  • 差分输入时要注意共模输入电压在中点附近,具体看说明书的共模输入