Other Parts Discussed in Thread: ADS1232
您好!我最近在使用ADS1232做一个电子称时遇到下面的问题,请指点: 1,我使用的是数据手册上的P25中的figure 42.因为我用的MCU是5V供电的,所以图示中的3V电源也是5V,也就是电路中的电源就只有一个5V实现,但是我在使用中发现,MCU能够检测到数据准备好信号,只是程序读出的24位数据全是1。我把ADS1232的11,12脚短接了输了出还是全是1,我给ADS1232的11,12脚外接输入一个差分3毫伏的信号,输出还是全1。我想是不是这个芯片坏了。(我没有做电路板,只是用一个贴片转直插的板子,将ADS1232转成直插用万能板接成图示电路)。 2,我在数据手册上看到P18关于此转换器的LSB的定义感到不能理解:0.5VREF/(223 – 1).这里的分母为什么要减个1呢,我觉得不应该减1啊? 谢谢指点 2014.2.20